MITSUBISHI ELECTRIC Changements pour le meilleur
Power Industry

Digital transformation in the energy sector

10.07.20264 minutes de lecture

The global energy landscape is currently undergoing its most significant shift since the dawn of electrification. As the world moves towards carbon neutrality, the traditional model of centralised power generation is being replaced by a complex, decentralised, and highly volatile ecosystem. In this context, the digital energy industry has emerged as the only viable path forward. Digital transformation is no longer a choice for utility companies; it is a fundamental requirement for survival in an era defined by decarbonisation, decentralisation, and the urgent need for operational resilience.

Introduction to digital transformation in the energy sector

Digital transformation in the energy sector refers to the integration of advanced digital technologies - such as the Industrial Internet of Things (IIoT), Artificial Intelligence (AI), and big data analytics - into every aspect of power generation, transmission, and distribution. It represents a move away from mechanical infrastructure towards a connected energy systems model where data is as valuable as the electricity itself.

For decades, the power industry operated on a simple principle: generate power in large, fossil-fuelled plants and send it one way to the consumer. Today, that model is broken. The rise of intermittent renewables like wind and solar, the growth of electric vehicle (EV) charging networks, and the emergence of "prosumers" (consumers who also generate their own power) have created a grid that is increasingly difficult to manage manually. The future of energy industry depends on our ability to create a "smart" grid that can balance itself in real-time. This is where digital transformation in power industry becomes critical, providing the tools needed to manage complexity while improving efficiency and reducing environmental impact.

Challenges facing modern energy companies

Modern energy companies are operating in a "perfect storm" of challenges. The most immediate pressure is the global drive for sustainability. Governments around the world have set ambitious targets for carbon reduction, requiring a rapid shift away from coal and gas. However, integrating renewable energy is not a simple task. Unlike a coal plant, which can provide a steady "baseload," wind and solar are unpredictable. This volatility puts immense strain on aging infrastructure that was never designed to handle such fluctuations.

Furthermore, the sector is facing a significant decentralisation of assets. Instead of a few hundred large power plants, we now have millions of small energy sources, from rooftop solar panels to community wind farms. Managing this fragmented landscape requires a level of coordination that traditional energy management technologies simply cannot provide.

Finally, there is the challenge of aging assets and a retiring workforce. Many power plants are operating on legacy systems that are decades old, making them prone to failure and difficult to maintain. At the same time, the "tribal knowledge" of experienced engineers is disappearing as they retire. Digital utilities transformation is essential to capture this knowledge in digital systems and to provide the predictive capabilities needed to keep old assets running safely and efficiently.

The client’s operational and energy management issues

To understand the impact of digitalisation, we must look at the typical operational issues faced by energy companies today. Many organisations still rely on "siloed" data. Information from the boiler room doesn't talk to the turbine control system, and neither of them is connected to the grid management office. This lack of visibility leads to significant inefficiencies.

Common issues include:

  • Reactive maintenance: Equipment is often repaired only after it fails, leading to expensive unplanned outages and emergency repair costs.

  • Manual data collection: In many legacy plants, operators still walk around with clipboards, manually recording temperatures and pressures. This is slow, prone to error, and provides no real-time insight.

  • Inefficient load balancing: Without smart grid automation, companies struggle to match supply with demand in real-time, often leading to wasted energy or the need to buy expensive "peaker" power from the market.

  • Lack of traceability: Meeting environmental regulations requires precise reporting on emissions and fuel usage. Manual systems make this documentation process incredibly burdensome and risky.

    These issues collectively result in higher operational costs, lower reliability, and a reduced ability to compete in a modern, digital energy industry.

Objectives of the digital transformation strategy

A robust digital transformation strategy must be built on clear, measurable objectives. For most energy companies, the primary goal is to improve "flexibility." In a world of renewables, a power plant must be able to ramp up or down quickly without damaging its equipment.

The core objectives typically include:

  • Enhanced grid stability: Using smart grid technologies to ensure that the supply of electricity always matches the demand, regardless of weather conditions.

  • Operational excellence: Moving from reactive to predictive maintenance to reduce downtime and extend the life of critical assets.

  • Cost optimisation: Reducing fuel consumption and operational overheads through data-driven energy management.

  • Sustainability: Providing the transparency needed to meet carbon reduction targets and integrate higher levels of renewable energy.

  • Cyber resilience: Ensuring that as the plant becomes more connected, it remains protected against the growing threat of cyber-attacks on critical infrastructure.

    By achieving these objectives, companies can transition from being traditional utilities to becoming leaders in the future of energy industry.

Implemented digital technologies and automation solutions

The transition to a digital power plant requires a suite of integrated energy sector automation solutions. At the heart of this transformation is the Distributed Control System (DCS). Mitsubishi Electric’s PMSX®pro is a prime example of a high-availability DCS designed specifically for the power industry. It provides a unified platform for sequence control, process control, and electrical management, ensuring that every part of the plant is synchronised.

Another critical technology is the digital power generation systems used for turbine control. Solutions like the Turbiset control and protection system allow operators to upgrade aging turbines with modern, high-speed controllers. This not only improves efficiency but also provides the rigorous protection needed to operate 24/7.

Furthermore, smart energy infrastructure includes the deployment of Virtual Power Plant (VPP) controllers. These systems allow a company to coordinate a variety of decentralised assets - such as a mix of wind, solar, and battery storage - to act as a single, reliable power source. This level of industrial automation in energy sector is what allows for the reliable integration of renewables into the national grid. For more details on these technologies, visit our Power industry solutions page.

The role of Industrial IoT and data integration

The Industrial IoT in energy sector is the "nervous system" of the modern power plant. By deploying thousands of smart sensors across the facility, companies can collect "big data" on everything from vibration and temperature to fuel flow and emissions. However, data alone is not enough; it must be integrated.

Data-driven energy management relies on breaking down the silos between Information Technology (IT) and Operational Technology (OT). When sensor data from the shop floor is integrated with business systems (like ERP or weather forecasting tools), the plant becomes truly "intelligent." For example, a plant can automatically adjust its output based on a forecast of cloud cover affecting solar production elsewhere in the grid.

This level of connectivity is a core component of the wider energy systems solutions provided by Mitsubishi Electric. By using open communication protocols, these systems ensure that data flows seamlessly from the smallest sensor to the executive dashboard, providing a "Single Version of the Truth" for the entire organisation.

How smart energy infrastructure improved operational efficiency?

The implementation of smart energy infrastructure has a direct and immediate impact on operational efficiency. One of the most significant improvements is in the area of "heat rate" optimisation. In thermal power plants, even a 1% improvement in efficiency can lead to millions of pounds in fuel savings and a massive reduction in CO2 emissions.

Smart grid automation also improves efficiency by reducing "line losses" during transmission. By using AI to optimise the flow of electricity across the grid, utilities can ensure that power takes the most efficient path to the consumer.

Furthermore, digitalisation improves the efficiency of the workforce. With remote monitoring and mobile HMI solutions, engineers no longer need to be physically present at every asset to perform inspections. They can monitor the health of a wind turbine or a substation from a central control room, only deploying maintenance teams when the data indicates a genuine problem. This transition to a digital utilities transformation model allows companies to do more with fewer resources.

Results achieved through energy sector digitalisation

The results of energy sector digitalisation are measurable and profound. Companies that have successfully implemented digital transformation in power industry strategies typically report:

  • Reduced unplanned downtime: By using predictive maintenance, plants can identify potential failures weeks in advance, reducing emergency outages by up to 50%.

  • Lower operational costs: Automation reduces the need for manual intervention and optimises fuel usage, leading to a significant improvement in the bottom line.

  • Faster response times: Smart grid technologies allow the grid to respond to disturbances in milliseconds, preventing large-scale blackouts.

  • Improved compliance: Automated reporting ensures that environmental and safety documentation is always accurate and ready for audit.

    These results prove that the digital energy industry is not just a theoretical concept; it is a high-performance reality that delivers a clear Return on Investment (ROI).

Benefits for productivity, sustainability, and cost optimisation

The benefits of digitalisation can be categorised into three main pillars: productivity, sustainability, and cost optimisation.

  • Productivity: Industrial automation in energy sector allows for 24/7 operation with minimal human error. It enables "online engineering," where systems can be updated or expanded without shutting down production. This ensures that the plant is always operating at its maximum possible capacity.

  • Sustainability: Digitalisation is the "green engine" of the energy sector. It provides the tools needed to balance the grid as we integrate more renewables. By reducing fuel waste and optimising combustion, it directly supports global carbon reduction goals.

  • Cost optimisation: Beyond fuel savings, digitalisation reduces the "Total Cost of Ownership" (TCO) of energy assets. Predictive maintenance extends the life of expensive machinery, delaying the need for multi-million-pound capital replacements.

    These benefits are similar to those achieved in other resource-heavy industries. For example, you can see how similar principles are used for Reducing energy costs in the water industry.

Key lessons learned from the digital transformation process

After years of implementing energy sector automation solutions, several key lessons have emerged. First, digital transformation is not just about technology; it is about people. Success requires a culture of continuous learning and a willingness to move away from "the way we've always done it."

Second, start with a clear problem. Don't just "buy AI" because it's a trend. Identify your biggest bottleneck - whether it's unplanned downtime or inefficient fuel usage - and apply the technology there first.

Third, data integrity is paramount. A data-driven energy management system is only as good as the data it receives. Investing in high-quality sensors and robust industrial networks is the essential first step.

Finally, remember that digitalisation is a journey, not a destination. The future of energy industry will continue to evolve, with new technologies like blockchain and hydrogen storage on the horizon. A flexible, scalable digital foundation is the only way to ensure your organisation is ready for whatever comes next. For more insights on this ongoing transformation, read our article on Smart energy management in modern manufacturing.

FAQ section

What is digital transformation in the energy sector?

It is the integration of digital technologies like IIoT, AI, and cloud computing into power generation and distribution. This creates a digital energy industry where data is used to optimise efficiency, integrate renewables, and improve grid stability.

How does digitalisation improve energy management?

Digitalisation provides real-time visibility into every asset. By using data-driven energy management, companies can identify waste, predict maintenance needs, and automatically balance supply and demand, leading to lower costs and higher reliability.

What technologies are used in smart energy infrastructure?

Key technologies include Distributed Control Systems (DCS) like PMSX®pro, SCADA systems, Industrial IoT sensors, AI-driven analytics, and Virtual Power Plant (VPP) controllers that coordinate decentralised energy sources.

What are the benefits of automation in the energy industry?

Automation improves safety by providing rapid protection against faults, increases efficiency by optimising combustion and load balancing, and reduces costs by enabling predictive maintenance and reducing manual intervention.

How does Industrial IoT support digital energy solutions?

The industrial iot in energy sector provides the sensory data needed for intelligent decision-making. It connects thousands of devices, allowing for remote monitoring, performance benchmarking, and the implementation of advanced AI algorithms.

Why is data integration important in energy management?

Energy plants are complex. Data integration breaks down the silos between different systems (like the turbine and the grid), providing a holistic view that is essential for smart grid automation and efficient operation.

What challenges do energy companies face during digital transformation?

Major challenges include integrating with legacy (aging) infrastructure, overcoming internal resistance to change, ensuring cybersecurity in a connected environment, and managing the massive volumes of data generated by IoT devices.

What is the future of digital transformation in the power industry?

The future of energy industry lies in fully autonomous "self-healing" grids, the widespread use of digital twins for real-time simulation, and the integration of AI to manage a 100% renewable energy ecosystem.


Articles similaires


Sujets

Power Industry