MITSUBISHI ELECTRIC Changements pour le meilleur
Water / Waste Water

Smart water treatment plants

17.07.20263 minutes de lecture

As global water demands rise and climate change intensifies, traditional water facilities face unprecedented pressure. Modern water utilities must transition from manual, reactive operations to resilient, automated systems. By embracing digital transformation, plants can secure water quality, optimise energy use, and address critical labor shortages.

What are smart water treatment plants?

Smart water treatment plants represent the future of digital water treatment, transforming traditional facilities into highly connected systems. By integrating a resilient smart water infrastructure, these plants shift from reactive operations to proactive, automated management. Utilising connected sensors and intelligent networks, they secure water quality, optimise resources, and ensure uninterrupted distribution across municipal networks.

Key technologies behind intelligent water treatment systems

Key technologies behind intelligent water treatment systems

Modernising facilities requires advanced water management technologies. Similar to the automation principles deployed in the first sustainable metal recycling plant, the core of the industrial IoT in water sector relies on:

  • Edge & Control: High-performance MELSEC programmable controllers (PLCs) managing local processes.
  • Visualisation: The ICONICS Software Suite (GENESIS 11), providing real-time operational visibility and centralised control.
  • Archiving: Hyper Historian logging mission-critical data.
  • Smart Drives: FREQROL variable speed inverters optimising motor operations.

Real-time water quality monitoring and data analytics

Deploying connected water systems allows utilities to transition to data-driven water management. Live telemetry data and continuous monitoring of water sources provide operators with immediate insights into chemical levels and flow rates. This real-time visibility enables instant countermeasures, boosting overall plant performance and ensuring regulatory compliance.

How AI and machine learning improve water treatment operations?

Integrating AI in water industry directly addresses critical challenges like skilled labor shortages.

  • Predictive maintenance: AI-enabled FREQROL inverters self-diagnose mechanical anomalies, such as bearing wear or corrosion, before failures occur.
  • Knowledge transfer: Expert systems capture the intuition of experienced operators, assisting new staff in daily operations.

Industrial water treatment automation and process optimisation

Implementing comprehensive water treatment automation is key to optimising energy-intensive processes like aeration and pumping. Combining high-efficiency motors with smart software like EcoAdviser, utilities can identify underperforming assets and eliminate energy waste. This level of industrial automation in water sector ensures cost-effective operations.

What are the benefits of digital water treatment plants?

The digital utilities transformation delivers measurable operational and environmental advantages through water sector automation solutions:

  • Energy savings: Advanced monitoring and variable speed drives lower electricity consumption.
  • Asset longevity: Backwards-compatible hardware upgrades maximise the lifespan of legacy systems.
  • Resource conservation: Precise process control minimises water loss and chemical overuse.
  • Climate resilience: Real-time environmental data helps mitigate risks from droughts or heavy rainfall.

Challenges of implementing smart water management systems

Executing a successful digital transformation in water industry requires addressing key integration and security challenges.

  • Cybersecurity: Protecting critical infrastructure demands a holistic "Defense-in-depth" strategy, certified under IEC 62443-4-1.
  • Ageing Infrastructure: Integrating legacy assets with modern platforms can be complex.
  • To minimise risks and engineering costs when upgrading your plant, utilities should adopt a step-by-step approach using the Smart Manufacturing Kaizen Level (SMKL) methodology.

FAQ section

What are smart water treatment plants?

Smart water treatment plants are modern, highly automated facilities that leverage smart water technologies - such as IoT sensors, edge controllers, advanced SCADA systems, and artificial intelligence - to monitor, control, and optimise water purification and distribution processes. Unlike traditional plants that rely on manual sampling and reactive adjustments, smart plants collect and analyse real-time operational data. This allows them to dynamically adjust chemical dosing, optimise pump speeds, and detect quality anomalies instantly, ensuring a safe, reliable, and highly efficient water supply.

How do intelligent water treatment systems work?

These digital water systems operate through a multi-layered digital architecture. At the field level, smart sensors and instruments continuously gather real-time data on parameters like pressure, flow, pH, and turbidity. This data is transmitted to edge controllers (such as MELSEC PLCs) that execute precise, localised control loops. The information is then aggregated by advanced SCADA platforms (like the GENESIS 11) for centralised visualisation and enterprise-wide monitoring, allowing operators to make data-driven decisions and respond proactively to changing conditions.

What technologies are used in smart water treatment plants?

Just like advanced industrial facilities - such as the first sustainable metal recycling plant - modern water plants rely on a combination of robust hardware and intelligent software. Key technologies include programmable logic controllers (PLCs) for local process control, variable speed drives (VFDs) like FREQROL to optimise pump and motor efficiency, high-speed data archives (Hyper Historian) to securely log massive volumes of telemetry data, and AI-driven data science tools to perform real-time diagnostics and predictive maintenance.

What is real-time water quality monitoring?

Real-time water quality monitoring is the continuous, telemetry-driven tracking of physical, chemical, and biological water parameters. In traditional water treatment setups, operators manually collect samples and test them in a laboratory, which introduces significant delays. Real-time monitoring uses connected inline sensors to provide instantaneous data on parameters such as chlorine levels, turbidity, and dissolved oxygen. This allows utilities to immediately detect contamination, adjust chemical treatment on the fly, and prevent hazardous water from entering the distribution network.

How is AI used in water treatment plants?

In modern water systems, AI in water industry is primarily used for predictive maintenance, process optimisation, and knowledge transfer. AI algorithms analyze real-time data streams from critical assets (like pumps and blowers) to identify early signs of wear and tear - such as bearing degradation or corrosion - before a failure occurs. Additionally, AI-driven data science tools automate complex data analysis, allowing operators to optimise energy-intensive processes like aeration and pumping without requiring specialised data scientists.

What are the benefits of automated water treatment systems?

Automated systems deliver measurable operational, financial, and environmental advantages through water sector automation solutions. They significantly reduce energy consumption by dynamically adjusting pump and blower speeds to match actual demand. They also minimise chemical waste through precise automated dosing, prevent costly unplanned downtime through predictive alerts, and simplify regulatory compliance by generating accurate, real-time reports. Furthermore, automation enhances climate resilience, allowing plants to automatically adapt to sudden capacity surges during heavy rainfall or manage resources during droughts.


Sujets

Water / Waste Water