MITSUBISHI ELECTRIC Changements pour le meilleur
Material handling

Warehouse automation and smart logistics

07.08.20263 minutes de lecture

The rapid expansion of e-commerce and shifting supply chain demands have placed unprecedented pressure on distribution centers. To maintain a competitive edge, facilities must transition from manual, error-prone workflows to agile, automated systems. Implementing advanced logistics automation is a strategic necessity to ensure continuous throughput, maximum accuracy, and operational resilience.

Why this warehouse needed to rethink Its logistics operations?

Before modernising, the facility struggled with severe bottlenecks in its manual picking and kitting departments. High employee turnover and complex, high-mix product orders led to frequent picking errors, which slowed down shipments and increased reverse logistics costs. The warehouse relied on paper-based tracking, making real-time inventory management impossible. To scale operations and eliminate costly human errors, the facility needed a comprehensive warehouse digitalisation strategy to replace its outdated, manual workflows.

Warehouse automation systems implemented: what was deployed and why?

The facility deployed a suite of automated warehouse solutions designed to eliminate errors at the source. They integrated Guided Operator Solutions (GOS) for mistake-proof picking, kitting, and parts replenishment. These Poka Yoke terminals guide workers to the correct parts bin using light indicators, photoelectric sensors, and physical shutter doors that only open for the correct item. To revolutionise transport, the warehouse implemented the Linear Transfer System (LTS) with Smart Carriage technology. Developed with APT Automation, these intelligent carriages travel up to 4m/s with payloads up to 12kg. Equipped with 24VDC onboard power, they power sensors and grippers in transit. Similar to the advanced control systems running the first sustainable metal recycling plant, this setup allows seamless synchronisation with MELFA industrial robots.

How smart warehouse technology changed daily operations?

Integrating smart warehouse technology completely transformed daily workflows. Operators now monitor the entire facility through the ICONICS GENESIS 11 SCADA platform, which aggregates data from field devices into intuitive, real-time dashboards. This seamless integration of IIoT in logistics connects the warehouse floor directly to ERP and MES systems over high-speed CC-Link networks. Daily operations also became safer. The LTS features an Advanced Safety System with Safety Zone Scanners that reduce carriage speed when an operator is detected, allowing the system to operate in a fenceless environment. Furthermore, by adopting a step-by-step SMKL methodology when upgrading your plant, the warehouse minimised implementation risks.

Results: what logistics automation delivered in numbers?

The transition to smart logistics systems delivered immediate, measurable improvements. Picking errors were completely eliminated, reducing return processing costs by 95%. The combination of GOS and LTS increased picking speeds by 45%, significantly boosting overall performance. Additionally, the warehouse achieved a 30% increase in throughput by deploying these advanced material handling automation solutions, proving that predictive logistics automation and modern warehouse robotics deliver a rapid return on investment.

FAQ section

What are warehouse automation systems and how do they work?

They are integrated hardware and software solutions - such as conveyors, AMRs and smart picking terminals - that automate repetitive warehouse tasks. Coordinated by SCADA platforms like GENESIS 11, they translate ERP orders into physical movement paths to store, retrieve, and sort goods with absolute precision.

How does logistics automation reduce operational costs?

Automation cuts costs by virtually eliminating picking errors, optimising labor utilization, and maximising vertical storage space. Additionally, predictive diagnostics identify equipment wear early, preventing expensive emergency repairs and unplanned downtime.

What is smart warehouse technology?

Smart warehouse technology integrates IIoT sensors, artificial intelligence, and real-time data analytics into traditional operations. This enables systems to adapt dynamically to changing conditions, such as predicting bottlenecks, reconfiguring routes, and self-diagnosing machinery.

How long does a warehouse automation implementation typically take?

Implementation timelines range from a few weeks for targeted upgrades (like Guided Operator Solutions) to 12–18 months for facility-wide overhauls. Using a step-by-step SMKL methodology allows companies to scale gradually and minimise operational disruption.

What should companies consider before investing in logistics automation?

Companies should evaluate their current operational bottlenecks, ensure system interoperability over high-speed networks like CC-Link, and prioritise modular scalability. They must also consider safety compliance for fenceless environments and calculate the long-term total cost of ownership.


Articles similaires


Sujets

Material handling