MITSUBISHI ELECTRIC Changements pour le meilleur

In this case study...

  • Turning energy data into actionable insights,
  • Simplified reporting with greater transparency,
  • Faster responses to changing energy demands,
  • Supporting sustainability through digitalisation,
  • Building a foundation for continuous optimisation.

For more than 120 years, Rauschert has excelled in high‑precision technical ceramics. As the company modernizes its operations, energy transparency has become increasingly important — especially with growing reporting requirements and the desire for continuous efficiency improvements.To support this evolution, Rauschert implemented Mitsubishi Electric’s GENESIS Energy Management Platform, unlocking real‑time clarity across all facilities.

The Challenge: Bringing clarity to a complex energy landscape

For more than 120 years, Paul Rauschert Steinbach GmbH has combined manufacturing expertise with a commitment to continuous improvement. While its production processes had evolved successfully over generations, energy management remained limited by an outdated monitoring system that offered little visibility into actual consumption patterns. 

Energy data was dispersed across multiple buildings and systems, making it difficult to identify the causes of consumption peaks or uncover opportunities for optimisation. Reporting was equally challenging, requiring the manual preparation of extensive spreadsheets every month, while growing regulatory requirements added further administrative pressure.

The Solution: GENESIS brings transparency and control

To gain better control of its energy usage, Paul Rauschert Steinbach GmbH implemented Mitsubishi Electric’s GENESIS Energy Management platform. The solution created a centralised environment for energy monitoring, reporting and analysis while integrating seamlessly with existing metering infrastructure. 

With real-time monitoring and intuitive visualisation tools, the platform enables operators to track energy consumption across the entire facility and quickly identify unusual patterns or inefficiencies. Advanced analytics, automated reporting and historical data storage provide the foundation for more informed operational and sustainability decisions.

What the platform delivers:

  • Universal Connectivity: All energy and utility meters feed into one secure, central data platform — without needing to replace existing hardware.
  • Real‑Time Visibility Across the Entire Site: Teams can instantly identify consumption trends and trace anomalies from building‑level down to individual equipment.
  • Intelligent Analytics & Visualization: Dashboards, KPIs, power‑flow diagrams and asset‑based drill‑downs highlight inefficiencies and optimization opportunities.
  • One‑Click Reporting & EU Compliance: Automated consumption, cost, carbon and compliance reports replace time‑intensive manual processes.
  • Fast Deployment & Long‑Term Scalability: Because GENESIS is compatible with multiple meter types, implementation was quick — and the system is ready for future expansion.

The Result: Faster insights, smarter decisions

The project transformed energy management from a manual, time-consuming process into a proactive, data-driven activity. Instead of relying on lengthy spreadsheet reports, facility teams now have immediate access to actionable insights through a single, comprehensive view of energy performance.

Tasks that previously required hours of investigation can now be completed in minutes, helping teams identify the source of energy peaks faster and respond more effectively. Automated reporting has also simplified compliance processes, reducing administrative effort while improving access to accurate information.


Why it matters?

Many manufacturers face the challenge of improving energy efficiency without disrupting established operations. This project demonstrates how modern energy management technologies can unlock valuable insights from existing infrastructure, helping organisations reduce complexity, improve decision-making and support long-term sustainability goals. Through scalable digital tools and enhanced visibility, manufacturers can turn energy data into a strategic asset for future growth.

“The difference is remarkable. What used to require dedicated personnel and hours of manual work now provides instant analysis and useful insights.”— Fabian Völk, Maintenance & Engineering, Rauschert

Discover the solutions behind this case study

Ready to transform your energy management?

Turn complex energy data into actionable insights — without changing your existing infrastructure.

Have we sparked your interest? Contact us

0/255

En remplissant ce formulaire, vous consentez à ce que les données saisies soient traitées par la société MITSUBISHI ELECTRIC EUROPE B.V. et/ou ses sous-traitants, en tant que responsable de traitement aux fins de l’organisation et de la mise en œuvre de la formation en question. Les participants bénéficient d’un droit d’accès, de rectification, d’effacement (droit à l’oubli), de limitation de traitement, d’opposition et de portabilité sur les données personnelles les concernant. Dans l’hypothèse où les participants souhaiteraient exercer l’un de ces droits, ils devront en faire la demande auprès de MITSUBISHI ELECTRIC EUROPE B.V. par courrier électronique à l’adresse suivante: LDPC.France@fra.mee.com Notre politique de confidentialité est accessible via le lien suivant: fr.mitsubishielectric.com/fa/privacy

Les champs marqués d'un * sont obligatoires.

Our Stories

2025-09-01

Transforming energy management with real‑time insights

Paul Rauschert Steinbach GmbH

ENDE
#Manufacturing#Energy#Sustainability#GENESIS64