MITSUBISHI ELECTRIC Changements pour le meilleur

Turning data into energy awareness

Goal Challenge 
Building transparency around energy consumption to enable smarter decisions and engage employees in driving efficienc and CO₂ reductionWithout measuring energy use, inefficiencies remain hidden—and employees lack the awareness and motivation to engage. Yet starting across the board is overwhelming, making it unclear where to begin

The right reporting materials will guide the way

To effectively cut emissions, we need to raise the awareness of employees regarding energy saving. But what is the best way to achieve this?

Start by measuring the factory’s electricity, gas, and heavy oil consumption using various measuring instruments. With the right tools, this data is automatically collected by a dedicated data collection server, allowing CO₂ emissions to be monitored via a specialized web-based interface.

Continue
by using a dashboard screen to generate reporting materials that support CO₂ reduction activities and track progress effectively.
This will make it easier for employees to understand energy consumption and identify opportunities for energy savings.

EcoWebServerⅢ, an energy-saving data collection server, offers a simple solution for managing CO₂ emissions. It measures energy usage from electrical equipment such as switchboards and distribution panels, as well as gas and heavy oil consumption in boilers. Using CO₂ conversion factors, it calculates and tracks emissions by individual departments, line and product type as well as for an entire factory or individual building, laying the path for improved management.
Additionally, the EcoAdviser Graph and Dashboard functions allow users to create custom screens, making energy data visible to everyone and promoting awareness.

Contact us for more information about EcoWebServerⅢ

0/255

En remplissant ce formulaire, vous consentez à ce que les données saisies soient traitées par la société MITSUBISHI ELECTRIC EUROPE B.V. et/ou ses sous-traitants, en tant que responsable de traitement aux fins de l’organisation et de la mise en œuvre de la formation en question. Les participants bénéficient d’un droit d’accès, de rectification, d’effacement (droit à l’oubli), de limitation de traitement, d’opposition et de portabilité sur les données personnelles les concernant. Dans l’hypothèse où les participants souhaiteraient exercer l’un de ces droits, ils devront en faire la demande auprès de MITSUBISHI ELECTRIC EUROPE B.V. par courrier électronique à l’adresse suivante: LDPC.France@fra.mee.com Notre politique de confidentialité est accessible via le lien suivant: fr.mitsubishielectric.com/fa/privacy

Les champs marqués d'un * sont obligatoires.

What do you get out of it?

By using the right measuring instruments to track electricity, gas, and heavy oil consumption, energy management becomes more centralized and efficient. Automating data collection and CO₂ conversion significantly reduces the time and effort required for calculating energy use and emissions. A well-designed dashboard helps employees easily understand CO₂ emissions and energy-saving efforts, increasing awareness and engagement. Additionally, it streamlines the process of preparing internal reports on CO₂ reduction results, saving valuable labor time.

Product lineup