MITSUBISHI ELECTRIC Changements pour le meilleur

Complex production processes

The inherent complexity of food and beverage manufacturing, including variations in recipes, ingredient characteristics and packaging makes it difficult to clearly see the whole process end-to-end. Additionally, there can also be difficulties when it comes to automating tasks that involve intricate, non-repetitive motion.
Automation solutions address these challenges while providing transparency and affording manufacturers the ability to act responsively to problems or change.

Considerations for your production process

Visualise the invisible

Grasping the operational "picture" in a single glance is one of the challenges of the production manager. To do this, greater utilization of data networks and SCADA systems is required, even direct integration with the Manufacturing Execution Systems becomes essential.

Integration with Legacy Systems

Many food and beverage manufacturers have existing manual or semi-automated systems in place which cannot easily be changed. There are many challenges to seamlessly integrating new automation technologies with legacy systems. Sometimes they are connectivity based involving networks and protocols, sometimes process based involving digital twins and analysis and even sometimes human based, requiring support and training.

Sustainable manufacturing

Manufacturing sustainability relies on two fundamental aspects. The first is the resilience of the manufacturing process, achieved through efficient maintenance scheduling, proactive monitoring, and streamlined processes, all crucial for optimizing production efficiency and minimizing downtime. The second pillar is energy consumption, which directly impacts operational efficiency and underpins environmental responsibility. Sustainable energy management entails integrating it into automation processes to utilize energy efficiently and judiciously.

Optimise your process in the food & beverage industry

Dive deeper with in depth discussions or review one of our case studies below for more insights on this topic.

Product lineup

From keeping track of crucial machine KPI’s for enhanced OEE and productivity, to realtime remote asset monitoring. ​
Mitsubishi Electric’s Data Science Tool MELSOFT MaiLab is a data science tool that further improves manufacturing by replacing “human experience and intuition” with digital technology and enabling it to be easily incorporated into control systems.
Le robot collaboratif Mitsubishi Electric – MELFA ASSISTA – peut partager un espace de travail commun avec les opérateurs. Simplicité, Facilité et Flexibilité. Ce robot va changer votre perception sur la « robotique ».
Les servosystèmes de Mitsubishi - progressifs et modulables.

7 quick wins for an agile manufacture future

Many of the smart manufacturing ideas and strategies that are discussed assume a base level of automation and integration that are much easier to achieve in greenfield sites that have been built to be smart from the ground up.

However, there are a number of simple ideas that can be implemented with minimal time and cost that can have a big impact on addressing today’s manufacturing challenges.

Sign up and download white paper here

En remplissant ce formulaire, vous consentez à ce que les données saisies soient traitées par la société MITSUBISHI ELECTRIC EUROPE B.V. et/ou ses sous-traitants, en tant que responsable de traitement aux fins de l’organisation et de la mise en œuvre de la formation en question. Les participants bénéficient d’un droit d’accès, de rectification, d’effacement (droit à l’oubli), de limitation de traitement, d’opposition et de portabilité sur les données personnelles les concernant. Dans l’hypothèse où les participants souhaiteraient exercer l’un de ces droits, ils devront en faire la demande auprès de MITSUBISHI ELECTRIC EUROPE B.V. par courrier électronique à l’adresse suivante: LDPC.France@fra.mee.com Notre politique de confidentialité est accessible via le lien suivant: fr.mitsubishielectric.com/fa/privacy

Les champs marqués d'un * sont obligatoires.

Competencies

Our Stories

2026-01-26

NEWKFT Food Machinery Boosts Precision & Simplifies Architecture with CC‑Link IE TSN

KFT Food Machinery

EN
#Food & Beverage#Machine Building#Q series Motion controller#Inverters-FREQROL#Low-voltage Circuit Breakers#AC Servos-MELSERVO

2024-10-07

NEWInnovation in dairy production

Advanced Machine Company AS (AMC) x Tine SA

EN
Regardez la vidéo sur YouTube
#Machine Building#Food & Beverage

2024-08-01

From food waste to soil in 24 hours

Solserv AB

ENDE
Regardez la vidéo sur YouTube
#Food & Beverage#Machine Building#Sustainability#Energy#Visualization#Inverters-FREQROL#Controllers

2019-07-06

Robot duo cuts cakes & much more

Western Mechanical Handling (WMH)

DE
#Food & Beverage#Machine Building#AC Servos-MELSERVO#Human-Machine Interfaces (HMIs) - GOT#Industrial Robots - MELFA#Controllers

2019-01-10

Craft Brewery Automation

Sadler's Ales

2016-09-30

Optimisation of meat production

N&N Nadratowski

2016-07-01

Robot integration delivers precision cake slicing

Newtech Ltd

ENDE
Regardez la vidéo sur YouTube
#Food & Beverage#Human-Machine Interfaces (HMIs) - GOT#Controllers#Robots

2014-06-04

Dairy company in Regensburg

Bayernland eG

ENDE
#Food & Beverage#Controllers