MITSUBISHI ELECTRIC Changements pour le meilleur

In this case study...

  • Up to 600 products handled per minute
  • Dual-robot system for maximum throughput
  • Precise handling of fragile glass vials
  • Compact cell design saves valuable floor space
  • Consistent quality with high-speed automation

To address growing medicines shortages across Europe, Robotronic partnered with Mitsubishi Electric to revolutionise pharmaceutical packaging with cutting-edge robotics. By combining compact design, compliance control, and unmatched precision, they delivered a solution that ensures maximum productivity without compromising safety. This collaboration highlights how automation and robotics can solve critical supply chain challenges in the pharmaceutical industry.

The challenge: meeting pharmaceutical demand with precision and safety

Pharmacies across Europe are facing shortages of essential medicines, particularly children’s cough syrups. Increased demand is leaving shelves empty, calling for faster production and efficient packaging solutions. Robotronic, a Swiss company specialising in robotic applications for the pharmaceutical industry, needed to design compact, high-performance machines capable of handling fragile glass vials with precision and zero product damage—all while maintaining strict regulatory compliance.

The solution: compact, innovative robotics

Robotronic, in collaboration with Mitsubishi Electric, developed a compact robotic solution designed to maximise speed, precision and reliability. Using MELFA FR series robots, the system handles fragile glass vials with compliance control technology that virtually eliminates product damage. Dual-robot operation enables precise, high-speed processing in confined spaces, while integrated Mitsubishi Electric servos, PLCs and GOT HMIs ensure seamless and efficient machine performance.

The result: high-speed, damage-free production

The solution delivers zero product damage thanks to compliance control technology that ensures the gentle handling of glass vials and eliminates breakage. Its compact design allows machines to operate in spaces as small as 120 × 80 cm while processing up to 600 products per minute. Dual-robot operation enables two robots to work side by side with exceptional precision and long-term reliability, maintaining consistent performance over many years of operation. At the same time, the system meets the stringent safety and quality requirements of the pharmaceutical industry, ensuring full regulatory compliance.

Why it matters?

This project demonstrates how advanced robotics and strong partnerships can address critical challenges in the pharmaceutical industry. By combining Robotronic’s expertise in pharmaceutical processes with Mitsubishi Electric’s cutting-edge robotics, the collaboration delivered a solution that not only increases productivity but also ensures safety and reliability. As medicines shortages persist, such innovations are crucial for maintaining a resilient and efficient supply chain.

Discover the solutions behind this case study

Have we sparked your interest? Contact us

0/255

En remplissant ce formulaire, vous consentez à ce que les données saisies soient traitées par la société MITSUBISHI ELECTRIC EUROPE B.V. et/ou ses sous-traitants, en tant que responsable de traitement aux fins de l’organisation et de la mise en œuvre de la formation en question. Les participants bénéficient d’un droit d’accès, de rectification, d’effacement (droit à l’oubli), de limitation de traitement, d’opposition et de portabilité sur les données personnelles les concernant. Dans l’hypothèse où les participants souhaiteraient exercer l’un de ces droits, ils devront en faire la demande auprès de MITSUBISHI ELECTRIC EUROPE B.V. par courrier électronique à l’adresse suivante: LDPC.France@fra.mee.com Notre politique de confidentialité est accessible via le lien suivant: fr.mitsubishielectric.com/fa/privacy

Les champs marqués d'un * sont obligatoires.

Our Stories

2026-10-20

NEWRobotics and force sensing for intelligent testing of automotive components

Minebea Access Solutions

EN
Regardez la vidéo sur YouTube
#MELSOFT Gemini 3D Simulator#Industrial Robots - MELFA

2026-02-01

Can robots fill the pharmaceutical supply gap?

Robotronic

Regardez la vidéo sur YouTube
#Life Science#Industrial Robots - MELFA#Servo motors#Human-Machine Interfaces (HMIs) - GOT

2025-01-01

NEWMitsubishi Electric robot at Durable turns 25!

Durable

EN
#Manufacturing#Industrial Robots - MELFA

2024-06-01

Industrial robots as an unusual measuring tool for testing radar sensors

Noffz GmbH

ENDE
#Automotive#Digitalisation#Industrial Robots - MELFA

2022-12-01

Robotics‑powered decorative coating from a single source

Singulus Technologies AG

DE
#Packaging#Material Handling#Servo motors#Programmable Controllers MELSEC#Industrial Robots - MELFA

2019-07-06

Robot duo cuts cakes & much more

Western Mechanical Handling (WMH)

DE
#Food & Beverage#Machine Building#AC Servos-MELSERVO#Human-Machine Interfaces (HMIs) - GOT#Industrial Robots - MELFA#Controllers

2018-11-01

Poka Yoke: Error-free manual workstations

Werkstatt Bremen - Martinshof

DE
Regardez la vidéo sur YouTube
#Automotive#Material Handling#Controllers#Human-Machine Interfaces (HMIs) - GOT#Industrial Robots - MELFA