MITSUBISHI ELECTRIC Changements pour le meilleur

In this case study...

  • Faster troubleshooting with integrated diagnostics,
  • Improved reliability through star topology design,
  • Reduced commissioning with simpler configuration,
  • Simplified maintenance using standard Ethernet cabling,
  • Future-ready scalability for machine upgrades and expansion.

Every week, Huhtamaki’s Franeker plant in the Netherlands produces over 11 million molded-fiber egg cartons made from recycled paper. To keep this 24/7 operation running smoothly, the facility relies on highly automated production lines that must be fast, reliable, and ready for the future.To meet these demands, the plant is upgrading its automation infrastructure from legacy serial networks to CC‑Link IE Field, an open industrial Ethernet technology that delivers Gigabit performance, robust diagnostics, and long-term scalability. Already deployed across multiple production lines, the new network has significantly improved maintenance workflows, reduced troubleshooting time, and simplified system complexity—making it the new standard for future upgrades.

The challenge: keeping 24/7 production running without a single point of failure

Operating 24/7 production lines left little room for unplanned downtime. Huhtamaki Franeker's legacy serial network infrastructure offered limited diagnostics and relied on a daisy-chain topology, where a single cable failure could disrupt an entire production line. To support both existing equipment and future machine development, the plant needed a robust, future-ready automation platform based on Mitsubishi Electric iQ‑R series PLCs and CC‑Link IE Field, capable of delivering greater reliability, easier maintenance, and long-term scalability.

The solution: smarter diagnostics, less downtime

To support a more connected and future-ready production environment, Huhtamaki Franeker standardised on Mitsubishi Electric iQ‑R series PLCs, GOT HMI solutions, and the CC‑Link IE Field network. This unified automation platform provides a consistent foundation for machine modernisation, helping engineering teams work more efficiently while maintaining full visibility across operations. By bringing control, visualisation, and connectivity together within a single ecosystem, Huhtamaki has created a scalable approach that simplifies machine upgrades, supports evolving production requirements, and lays the groundwork for long-term operational excellence.

The result: Flexible, simplified network architecture

The modernised network infrastructure has given Huhtamaki Franeker greater flexibility to support evolving production requirements while simplifying day-to-day operations. Faster access to system information enables engineering teams to identify and address issues more efficiently, helping to minimise disruption in a demanding 24/7 manufacturing environment. At the same time, a more resilient network design has improved operational continuity and removed many of the limitations associated with the previous architecture. By adopting a standardised approach, the site has also made future upgrades, expansions, and maintenance activities easier to plan and execute, creating a strong foundation for long-term growth and continuous improvement.

Why it matters?

The new infrastructure simplifies maintenance and accelerates fault resolution, helping to minimise production disruptions and improve operational efficiency. With fewer components to manage and less time spent troubleshooting, engineering teams can focus on continuous improvement and future development rather than routine support activities.

Discover the solutions behind this case study

Have we sparked your interest? Contact us

0/255

En remplissant ce formulaire, vous consentez à ce que les données saisies soient traitées par la société MITSUBISHI ELECTRIC EUROPE B.V. et/ou ses sous-traitants, en tant que responsable de traitement aux fins de l’organisation et de la mise en œuvre de la formation en question. Les participants bénéficient d’un droit d’accès, de rectification, d’effacement (droit à l’oubli), de limitation de traitement, d’opposition et de portabilité sur les données personnelles les concernant. Dans l’hypothèse où les participants souhaiteraient exercer l’un de ces droits, ils devront en faire la demande auprès de MITSUBISHI ELECTRIC EUROPE B.V. par courrier électronique à l’adresse suivante: LDPC.France@fra.mee.com Notre politique de confidentialité est accessible via le lien suivant: fr.mitsubishielectric.com/fa/privacy

Les champs marqués d'un * sont obligatoires.

Our Stories

2026-07-07

NEWBMS-Driven energy and facility performance

Mitsubishi Electric Automotive Czech

EN
Regardez la vidéo sur YouTube
#Automotive#Mitsubishi Electric Iconics Digital Solutions#GENESIS64#MELSEC iQ-R Series

2026-02-01

Can robots fill the pharmaceutical supply gap?

Robotronic

Regardez la vidéo sur YouTube
#Life Science#Industrial Robots - MELFA#Servo motors#Human-Machine Interfaces (HMIs) - GOT

2026-01-26

NEWKFT Food Machinery Boosts Precision & Simplifies Architecture with CC‑Link IE TSN

KFT Food Machinery

EN
#Food & Beverage#Machine Building#Q series Motion controller#Inverters-FREQROL#Low-voltage Circuit Breakers#AC Servos-MELSERVO

2025-11-18

NEWEnhancing firefighter safety: from simulation to life-saving decisions

Fire GO GmbH

ENDE
Regardez la vidéo sur YouTube
#Data Collection/Analysis#Safety#Human-Machine Interfaces (HMIs) - GOT#Programmable Controllers MELSEC#MELSEC System Q

2025-08-18

CC‑Link Open Industrial Ethernet: Powering Reliable Production

Huhtamaki

EN
#Packaging#MELSEC iQ-R Series#Servo motors#AC Servos-MELSERVO#Inverters-FREQROL#Human-Machine Interfaces (HMIs) - GOT

2024-08-01

NEWFrom food waste to soil in 24 hours

Solserv AB

ENDE
Regardez la vidéo sur YouTube
#Food & Beverage#Machine Building#Sustainability#Energy#Visualization#Inverters-FREQROL#Controllers

2023-10-10

Printing Success: Futureproof and cost-effective solution

JK Machinery

#Machine Building#AC Servos-MELSERVO

2019-07-06

Robot duo cuts cakes & much more

Western Mechanical Handling (WMH)

DE
#Food & Beverage#Machine Building#AC Servos-MELSERVO#Human-Machine Interfaces (HMIs) - GOT#Industrial Robots - MELFA#Controllers